For more product information, click on the icons below

NEMA Type S Motor Starters (8536 8736 8606)
Available NEMA size 00-7 for non-reversing and NEMA size 00-5 for reversing electric motor applications

NEMA Fusible Disconnect Switch Combination Starters
NEMA size 0-6 with fusible or non-fusible disconnect switch

NEMA Circuit Breaker Combination Starters
NEMA sizes 0-7 with award-winning PowerPact circuit breakers