The PanelSeT SM floor standing steel enclosure are ideal for the Industrial, Energy and Infrastructure industry. The PanelSeT SM is made from a one single piece metal sheet, folded and welded on the corners for high robustness. The steel enclosures – PanelSeT SM offer the largest dimensional range in the market.
Floor standing steel enclosure, made from a one single piece metal sheet, folded and welded on the corners for high robustness. The steel enclosures – Spacial SM offer the largest dimensional range in the market. Find yours !
Characteristics
The steel enclosures – PanelSeT SM are capable of withstanding 600 kg distributed in their volume.
Material
Degree of protection
Certifications
IEC 62 208, BV rules for classification steel ships, DNV
Vibration Class A, UL & CUL 1,12 & 12K, NEMA 12 & 12K.
Schneider Electric selected a wide variety of spare parts for your enclosure. No matter if the enclosure is recently built or has several years, you can have the replacement parts you need.
The quick and simple solution
PanelSeT SM is the floor standing monobloc solution that provides: