EcoStruxure Control Expert Software

IEC programming software for Modicon PACs (formerly Unity Pro)

EcoStruxure Control Expert (formerly Unity Pro) is a unique software platform to increase design productivity and performance of your Modicon M340, M580 and M580 Safety, Momentum, Premium, Quantum applications.

Features

Unity Pro v10 Available Now
Within a single software package, Unity™ Pro development software allows the full development of applications including on-line updates and simulation with comprehensive debug functions.
This all-in-one software program is an integral part of the Schneider Electric Transparent Ready® product portfolio. From design to maintenance, Unity Pro optimizes operations by cutting development costs and reducing downtime across the application’s entire lifecycle. It allows users with multi-processor designs to share ideas and information visually, so individuals and teams can work together more effectively.

Unity Pro is multi-tasking software, offering the following features:

  • Support for the Quantum PAC, M580 ePAC, Premium PAC, M340 PAC, and the Momentum PLC
  • Conversion tools from legacy programs to new platforms
  • Standard and simple design with new IEC1131-3 features: Implicit Type Conversion and References
  • Cyber Security features to protect PLC and Unity Pro installations: Application password, Integrity Check, Access Control, and FTP/HTTP Control
  • Extended Trending Tool features: view and trace at PLC scan time
  • Free Companion tools: Unity Dif v8, EFB Toolkit v8, Unity Loader v10, and Advatys Configuration Software v8
  • Support for Altivar Process Drives with DTMs, embedded configuration tool, and delivered function blocks
  • Support for Microsoft Windows 7 (32/64 bits), Microsoft Windows 8.1 (32/64 bits), and Microsoft Windows Server 2012

Click to access the Unity Pro Selector Guide.

How to Videos

Creating and Using the DTX File in Unity Pro

 

Importing a Concept ASC File into Unity Pro

 

Configuring Totalizer FB in Unity Pro

 

Setting the IP Address on Modicon M340 with Unity Pro XL

 

Assigning an IP address to the BMXPRA0100 using Unity Pro

 

Creating Arrays with Unity Pro

 

Configuring L9 MSTR block in 984 ladder to read Modbus TCP device data

 

Viewing Installed Hotfixes in Unity Pro

 

Creating a 984LL segment section in Unity Pro

 

Updating Initial Values with Current Values in Unity Pro

 

Converting a ProWORX 32 Project to Unity Pro

 

How to Read and Convert 32 bit Signed Values

 

Setting Up DTM Browser for ModbusTCP Communication

 

Adding HART IO Devices on M580 with Unity Pro

 

Configuring IO Scanning on M580 in Unity Pro

 

Adding Ethernet-IP EDS file to DTM Library in Unity Pro

 

Using the MID INT function to extract character strings in Unity Pro XL

 

Adding a device profile to an AS-i configuration using Unity Pro

 

Configuration and Start Up of the EHC 0200 for Quadrature Mode

Benefits

Applications

  • Metals, Mining and Minerals
  • Material Handling
  • Oil & Gas
  • Water and Wastewater
  • Food & Beverage