Product Selectors are available to simplify selection of many Schneider products. Product Selectors provide a quick and easy way to determine the proper catalog number(s) required to meet a particular application, and also help identify compatible accessories. The selection process results in one or more catalog numbers, along with links to associated product information.

img Select a 'Product Subset'

In many cases more than one type of the selected product will be available. Start the selection process by specifying the 'product subset' required.

In some cases, Product Selectors may be launched with a Product Subset selected, bypassing this initial screen.

Once selected, the Product Subset will be displayed at the top of the Product Selector window. Selecting this link will return to the Product Subset selection screen.

 

img Complete Feature Selections

A number of Features are provided with value choices. Selecting values for these features will identify the parts required for your application.

·         As feature selections are completed, the available choices available for other features may be reduced based on those selections

·         If the list of available selections is reduced to a single answer, it is automatically selected

·         If your choices make a feature irrelevant to the application, the feature is removed from view

·         In some cases a hint may be provided to further explain the question

Values to individual features can be changed by selecting the corresponding  img  link.

The  img  link resets all answers so you can change your selections.

 

img Parts List

Once the required questions are answered a solution is provided. One or more parts are provided as the 'Parts' list.

In many cases, links are provided to access related documents such as datasheets and drawings.

These parts and quantities cannot be changed directly, but you can  img  your selections and start over.

 

 

img Accessories

Once a 'Final Parts List' solution is provided, additional accessories may also become available. Accessories are optional, but the displayed accessories wre compatable with your parts selection.

·         Select the corresponding  img  button to make accessory selections

·         Selecting the corresponding  img  button to remove a previous Accessory selection

·         In some cases you can specify/change the quantity by repeatedly pressing the  img / img  buttons, or by directly entering a quantity value.

·         Multiple accessories can be selected

Add these parts to my project

Once the Parts List and Accessories are selected, select the  img  button to complete the process.

The selected parts will be returned to your project system, and the Easy Selector will be closed.

Note: If you select the close button anytime during the selection process, the Easy Selector will be immediately closed, and no parts will be added to your project.

_