Safety controllers for safety applications requiring conformity up to Performance Level PL e/Category 4 EN ISO 13849-1 and SIL3 EN/IEC 61508
The Modicon range is part of the EcoStruxure Machine. The NEXT generation of EcoStruxure Machine, is an intuitive solution for machine automation with all the features and functions you need to build machines that will improve your bottom line. From design and development to commissioning and maintenance, EcoStruxure Machine is a complete machine-building solution with benefits throughout the machine life cycle. The Modular safety controllers Modicon MCM are designed to monitor multiple safety functions on and around a machine to minimize the risk of people accessing the dangerous moving parts of the machine such as:
Reduce time-to-market
Increase profitability
Improve efficiency
Simplify integration and maintenance