Flexible I/O expansion modules for M221, M241 & M251 Modicon PLCs. Includes digital and analog as well as mixed I/O. Also, includes special modules designed specifically for Machine Safety control. Up to 7 modules can be connected directly to the PLC. Also, the system can be expanded to include an additional set of 7 modules for a total of 14 modules and a couple hundred I/O points.
| Find Your Local Distributor (select High-Tech Distributors (ACE) from Choose an Activity drop down menu). |
Modicon TM3 I/0 system - your choice for flexible and customizable expansion of I/O terminals!
The specially developed Modicon TM3 I/O system enables flexible and customizable expansion of the I/O terminals in all of the controllers. Up to 14 terminals can be added to the controllers without tools. When the terminals are plugged in, their contacts are electrically linked to both the controller and the adjacent terminal. This high-speed expansion bus is 10 times faster than traditional solutions.
The Modicon TM3 offer provides a large range of I/O systems to enhance the capabilities of Modicon M221, M241, M251 logic controllers:
In addition, the Modicon TM3 expansion system is flexible due to the possibility of remotely locating some of the Modicon TM3 modules in the enclosure or another cabinet (up to 5 meters away, using a bus expansion system. It is common to the whole range of Modicon M221, M241 and M251 logic controllers, meaning that the model of controller can be revised without changing expansion module.
The Modicon TM3 is a MachineStruxure I/O system. The NEXT generation of MachineStruxureâ„¢ from Schneider Electric is an intuitive solution for machine automation with all the features and functions you need to build machines that will improve your bottom line. From design and development, to commissioning and maintenance, MachineStruxure is a complete machine building solution with benefits all through the machine life cycle.